This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
各位大大:
由于第一次发贴,如果格式错误,请提醒一下,我会改正;刚接触单片机不久,用的是msp430F5529的实验板,软件是ccs v5,想用定时器Time_A模块产生PWM信号用来对伺服电机进行位置控制。由于以前没有编程经验,所以在我搞明白定时器这部分原理以后,却发现很难下手去编程序。
我想求助一下大大们:能不能帮我找一点这方面的例程或者网址也行,让我可以参考着编一下,我从网上找了一些例子,发现如果将头文件改成msp430f5529.h以后,程序将不能运行,不知道是不是因为不是同一型号的单片机不能参考。
谢谢各位大大!
楼主:
给你发一个参考设计,用的F5xxx系列,但是都是类似。
如果你只想改一下芯片型号重新编译就能用,这是绝对不可能的,所以还是静下心来,学习啊。
Sensored 3-Phase BLDC Motor Control Using MSP430
http://www.ti.com/lsds/ti/microcontroller/16-bit_msp430/tools_software.page#code
dear fei shao:
我这里只有430G2XX系列的产考代码。我是在TI官网上下载的,上面的链接里面有对应的芯片型号及相应的code examples。
你可以下载430 software 安装后里面有所有系列的例程和应用文档,
下载链接http://www.ti.com/tool/msp430ware?DCMP=msp430ware&HQS=msp430ware
谢谢,我从ccs-welcome中的code-examples里面找到了例程,但是在我运行的时候发现了一个问题,我用P1.1和P1.2口作为pwm输出引脚(因为我看到资料上面说,定时器CCR1和CCR2做比较器是其输出引脚分别对应这两个),但是我从实验板上面找不到这两个引脚,不知道该怎么办才好。