This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADC悬空波形如何产生的



ADC应用没有问题,当输入信号板没接入时,每个通道都有不定的测量值,示波器观测有一个峰值1V左右,类似RC放电的波形,频率和采样频率一致。具体是如何产生的呢,为什么是峰值1V?参考电压是内部2.5V。谢谢,芯片是5438A

  • 配置为A/D的端口是不能悬空的,测试的时候一定要接入信号端.

    悬空状态时是有一定的电压与干扰,并不代表什么问题.所有单片机都这样.

  • 无图无真相。。。。。开玩笑啦,不过要看看这个波形是什么样子的?你是否扫描了多个通道,如果是多个通道的话看看这个5438A这个IC的ADC内部是否有一个采样保持电路(相当于一个电阻电容保持),在通道切换时这个保持电路还是在工作的,相当于就是有上一通道的电压残留在里面,不知道你的ADC输入阻抗要求怎样,如果阻抗没有什么要求的话(例采样点经过运放再到ADC),可以在这个ADC输入口接一个100K~1M的电阻来试试

  • ADC输入接口电路设计中必须有下拉或者上拉电阻,这样可以保证当ADC口没有信号输入时,处于一个固定的高电平或者低电平。