This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

我需要一些功耗测试数据



我需要一些功耗测试数据,证明MSP430功耗优于某些其他MCU,为什么应该选他,做仪表...

  • XinXin Li,

    MSP430不同系列的功耗时不同的,处于Active状态下时,其功耗如下,且此时BOR是一直开着的,且几乎是零功耗的。

    另外在MSP430还有7种Low Power Mode, 在LPM3下(此时MCLK和SMCLK均不可用,只有ACLk可用,且一般应用80%的时间处于此状态下,故LPM3下的低功耗和快速唤醒时间对平均功耗的进一步降低有很大意义),其功耗和唤醒时间如下,且在此模式下,BOR也是开着的。

    具体功耗数据,还是需要参考你具体选用MSP430型号的数据手册。

    另外,MSP430的低功耗不仅仅是CPU核的低功耗,外设也是本着低功耗原则设计的。

    希望对你有帮助!O(∩_∩)O~

  • 简单理解就是活跃状态下功耗很低并且在低功耗模式下功耗进一步降低,同时从低功耗唤醒到活跃状态的时间极小,这样就保证了MSP430整体的功耗极低!

  • 瞬时功耗有时候会变得很大,是什么原因呢... 比如从LPM3到Active时候,供电电池从3.6V一下子能降到3.0V,瞬间又好了