This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

如何将幅值大于3.3v的信号送入msp430进行AD转换

Other Parts Discussed in Thread: MSP430F5529

如何将幅值大于3.3v的信号(比如0-12v)送入msp430进行AD转换????用运放吗?还是电阻分压?电阻分压会不会导致采集结果不准?电阻阻值和标称值有点误差所致。

  • 用衰减输入信号的方法,就像万用表的原理,分档测量,大电压档用精密电阻做衰减器,不过这样会降低测量精度。或者直接用可编程运放,单片机多次采集测量,分析输入电压的范围,自动调整放大倍数,直至被测电压输入到A/D入口的电压接近基准源的最大值,这样测量的精度是最高的,不分档的全自动万用表就是这样工作的。

  • 如果采用电阻分压方式,标称值和实际值存在一定误差,可以选择高精度的电阻,也可以增加调校来校准其误差。

  • 在进行电阻分压的时候注意电阻值的大小,当电阻值很大时到达M级时相当于信号源的输出阻抗很大,这时就要增大单片机的采样保持的时间,使得AD测量准确~

  • 您好!在运用MSP430F5529的ADC时同样遇到了这样的问题,我的采样电压范围0V~4.2V,想用精密电阻分压,关于MSP430的ADC输入阻抗这一参数不清楚,所以分压电阻值不好确定,不知430的ADC输入阻抗是多少?分压电阻27K+100K是否合理?或给予推荐电阻值,谢谢!(论坛中相关的两个帖子查看过。)