This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430F5659 低功耗模式如何選擇?

Other Parts Discussed in Thread: MSP430F5659

Hi ALL:

  從MSP430F5659的datasheet中看到ActiveMode 下295µA/MHz at 8MHz,也就是295µA*8=2.36mA? 如果是以20MHZ的速度功耗就是5.9mA嗎?

  MSP430 有幾種低功耗模式,例如StandbyMode(LPM3),這時功耗2.2µA at 3.0V (Typical),但是這時CPU還能執行數據指令做數據處理嗎? 例如我們使用MSP430F5659做sensor數據採樣,採樣率為20mS,這20mS的時間間隔裏面大概有10mS的時間來做數據處理,是不是必須其中的10mS 以AM 模式運行,另外10mS才能使用低功耗模式?

 

BR

Wu Zhi-Rong

  • 您好! 5.9mA是CPU的最低功耗,如果以8MHz的主频,但是功耗还取决于你的模块配置以及外设的功耗。

    采样的等待过程中可以进入低功耗模式,数据处理只能在AM模式下。

    谢谢!