Part Number: MSP430FR5043
请问MSP430FR5043 气体测量的demo能提供一下吗?
官网没有找到相关的demo和软件
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
找过了下载提供的lib,MSP-USSSWLIB_Gas,但是里面只有430fr6043的demo没有5043的。就有个问题lnk430fr5043.xcl文件找不到,请问这个怎么怎么找或者怎么修改
430fr6043的demo设置修改到5043上,修改了一下芯片型号后编译出现错误请问怎么解决了
warning #10247-D: creating output section ".ram_thrill" without a SECTIONS specification
warning #10247-D: creating output section ".USS_ramfunc" without a SECTIONS specification
warning #10247-D: creating output section ".libVersion" without a SECTIONS specification
"../lnk_msp430fr5043.cmd", line 215: error #10099-D: program will not fit into available memory, or the section contains a call site that requires a trampoline that can't be generated for this section. run placement with alignment fails for section ".leaRAM" size 0xfa0. Available memory ranges:
LEARAM size: 0xec8 unused: 0xec8 max hole: 0xec8
error #10010: errors encountered during linking; "FR6043_USSSWLib_template_example.out" not built
前面3个,您没有为这些段指定内存分配,有关链接器命令文件的基础知识,请看:
https://software-dl.ti.com/ccs/esd/documents/sdto_cgt_Linker-Command-File-Primer.html
您也可以参考6043的进行修改。
第4个,给段.leaRAM分配的内存不够。