This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430 看门狗WDT的工作电流是多少?



请教!

MSP430 看门狗WDT的工作电流是多少?

  • MSP430的WDT的功耗实际就是开启时钟,让WDT的时钟源能够工作的功耗。WDT本身基本是不耗电的。

    具体的指标要看具体的芯片和你的代码来定。

    MSP430的WDT的时钟可以选择ACLK和SMCLK,而ACLK和SMCLK选择的振荡源不一样也会影响到功耗。

    以2系列的芯片为例,在LPM3 低功耗模式下WDT选择ACLK作为时钟源,ACLK在用外部32K晶体或者内部LF振荡源时的功耗典型值是:1.5UA和1.2UA。如果选择DCO作为振荡源,那么MCU就不能进入LPM3模式,这时的功耗就可能高达几十微安。所以根据你的需要选择合适的振荡源和时钟源才能最大限度地体现MSP430的低功耗特性。

    注:上面说到的功耗的值并不是单指WDT的值而是整个MCU的功耗,包含了brownout的功耗.