This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

msp430f5418a活动模式下功耗?

Other Parts Discussed in Thread: TPS61221, MSP430F5418A

最近在做一个项目设计,使用msp430f5418a单片机自制PCB测试版,使用外部晶振25MHz,系统时钟2分频,内核电压等级3(最高),开外设1路SPI(25M8分频),1路串口UART(115200波特率)。电源部分使用1节干电池通过TPS61221升至3.3V。估算单片机在活动AM模式下消耗电流10mA左右,是否正常?

msp430单片机的外设默认是不开启的吗?

该应用要求单片机基本处于活动AM模式下,是否能发挥msp430超低功耗的性能?

谢谢!

  • AM模式下 230uA/MHz 就芯片本身的电流应该会在几个mA. 10mA有点大,取决于外部设备的电流消耗。

    外设最好自己进行初始化。如果要降低功耗,尽量进入MSP430各种低功耗模式下来达到低功耗的设计。

  • 1.F5418A的动态模式功耗和低功耗模式功耗,在F5418A的datasheet第41页Electrical Characteristics中讲得很清楚,请参考。

    2.默认情况下有些外设是开启的,具体参加其user's guide的默认配置。

    3.MCU在12,5Mhz的动态模式,开启SPI,UART和其他外设的情况下,功耗是有可能到5-10mA的,同时DC/DC在这种情况下的效率较低,所以一般低功耗应用不推荐使用DC/DC方式供电,建议增加一节电池,选用LDO降压供电。

    4.超低功耗体现在三个方面,动态模式功耗的降低和时间缩短,低功耗模式的功耗低,AM与LPM的切换时间快。这三点MSP30都做得比较好,系统级的功耗就要靠系统软件设计来保证了,我们知道MCU最耗能的是CPU,所以在处理完任务后要及时关闭CPU和不用的高速外设,让MCU进入LPMx。