This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430的一点问题



研究MSP430单片机有一段时间了,有一下一些疑问,望高手指教: 
  ADC12内核时钟源ADC12OSC的频率是多少?如何确定?谢谢 
  采样保持信号源ADC12SC是否和ADC12OSC一样,他的频率又是多少,如何确定,谢谢。 
  就这几个,我查了好多资料都没讲到这点,谢谢高手帮忙,或者提供资料也可以。
  • Robert,你好,

    ADC12OSC是由MODOSC驱动的,大概有5MHz左右

    在2XX系列User's Guide中,关于ADC12OSC有这么一段描述:

    The ADC12OSC, generated internally, is in the 5-MHz range, but varies with individual devices, supply voltage, and temperature. See the device-specific datasheet for the ADC12OSC specification.

    不知道你用的是哪款芯片。

    所以请你查看一下datasheet中关于ADC12OSC的spec。

    ADC12SC是采样序列的触发,通过设置ADC12SC可以启动采样序列。频率与采样率有关系!

    希望我的回答对你有所帮助!

  • 谢谢你的回答,通过参考你的回答,我已经将这几个问题想清楚了,呵呵……