TI E2E™ 设计支持论坛将于 5 月 30 日至 6 月 1 日进行维护。如果您在此期间需要技术支持,请联系 TI 的客户支持中心寻求帮助。

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430G2755: uart example

Part Number: MSP430G2755
Other Parts Discussed in Thread: MSP430G2553

我在msp430G2755上写了一段uart串口通讯程序,但运行不成功,不知什么问题?

#pragma vector=USCIAB0RX_VECTOR
__interrupt void USCI0RX_ISR(void)
{
while (!(IFG2&UCA0TXIFG)); // USCI_A0 TX buffer ready?
if(UCA0RXBUF==2)
{instru[0]=2;
com_p=0;
}
else if(instru[0]==2)
{instru[++com_p]=UCA0RXBUF;
if(UCA0RXBUF==3||com_p>19)
com=1; // 命令结束
}
else
{instru[com_p]=UCA0RXBUF;
com_p++;
}
if(com_p>=29) com_p=0;
}

//////////串行口初始化
void ini_usart115k()
{
DCOCTL = 0; // Select lowest DCOx and MODx settings
BCSCTL1 = CALBC1_1MHZ; // Set DCO 0x86;//
DCOCTL = CALDCO_1MHZ; // 0xdb;//
P3SEL = BIT4 + BIT5 ; // P3.5 = RXD, P3.4=TXD
P3SEL2 = BIT4 + BIT5;
UCA0CTL1 |= UCSSEL_2; // SMCLK
UCA0BR0 = 8; // 1MHz 115200
UCA0BR1 = 0; // 1MHz 115200
UCA0MCTL = UCBRS2 + UCBRS0; // Modulation UCBRSx = 5
UCA0CTL1 &= ~UCSWRST; // **Initialize USCI state machine**
IE2 |= UCA0RXIE; // Enable USCI_A0 RX interrupt
}

  • 您好,请参考一下TI提供的例程:

    C:\ti\msp\MSP430Ware_3_80_14_01\examples\devices\MSP430G2xx\MSP430G2x55_Code_Examples\C

    SDK下载地址:https://www.ti.com.cn/tool/cn/MSPWARE

  • //////////串行口初始化
    void ini_usart115k()
    {
    DCOCTL = 0; // Select lowest DCOx and MODx settings
    BCSCTL1 = CALBC1_1MHZ; // Set DCO 0x86;//
    DCOCTL = CALDCO_1MHZ; // 0xdb;//
    P1SEL = BIT1 + BIT2 ; // P1.1 = RXD, P1.2=TXD
    P1SEL2 = BIT1 + BIT2;
    UCA0CTL1 |= UCSSEL_2; // SMCLK
    UCA0BR0 = 8; // 1MHz 115200
    UCA0BR1 = 0; // 1MHz 115200
    UCA0MCTL = UCBRS2 + UCBRS0; // Modulation UCBRSx = 5
    UCA0CTL1 &= ~UCSWRST; // **Initialize USCI state machine**
    IE2 |= UCA0RXIE; // Enable USCI_A0 RX interrupt
    }

    以上这段uart()初始化程序能够在msp430g2553上很好运行;后来我只是把P1,1和P1.2改成P3.4,P3.5就不能正常工作了;昨天我把tx和rx接到超级终端上检测,发现能够收到超级终端发出的字符,但超级终端不能收到2755发出的字符,检查寄存器UCA0TXBUF中的字符也是正确的,UCA0TXIFG置位也对,但不知何故就是没有输出信息?

    发送函数:

    int to232(char c) //发送一个字符
    {
    if(c<1||c>126) c='0';
    while (!(IFG2&UCA0TXIFG)); // USCI_A0 TX buffer ready?
    UCA0TXBUF = c; //
    return(c);
    }

  • 接线是正确的吗?

    G2553的P1.1是RXD,P1.2是TXD;G2755的P3.4是TXD,P3.5是RXD

  • 方便用示波器抓一下TX的波形吗?