请问 MSP430 LaunchPad 上的AD转换怎么在程序中调用啊?
怎么用C语言编写一个程序 “控制DDS输出的是一个固定频率的信号”。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
这是launch pad的ADC程序:
#include <msp430.h>
int main(void)
{
WDTCTL = WDTPW + WDTHOLD; // Stop WDT
ADC10CTL0 = SREF_1 + ADC10SHT_2 + REFON + ADC10ON + ADC10IE;
__enable_interrupt(); // Enable interrupts.
TACCR0 = 30; // Delay to allow Ref to settle
TACCTL0 |= CCIE; // Compare-mode interrupt.
TACTL = TASSEL_2 | MC_1; // TACLK = SMCLK, Up mode.
LPM0; // Wait for delay.
TACCTL0 &= ~CCIE; // Disable timer Interrupt
__disable_interrupt();
ADC10CTL1 = INCH_1; // input A1
ADC10AE0 |= 0x02; // PA.1 ADC option select
P1DIR |= 0x01; // Set P1.0 to output direction
for (;;)
{
ADC10CTL0 |= ENC + ADC10SC; // Sampling and conversion start
__bis_SR_register(CPUOFF + GIE); // LPM0, ADC10_ISR will force exi
if (ADC10MEM < 0x88) // ADC10MEM = A1 > 0.2V?
P1OUT &= ~0x01; // Clear P1.0 LED off
else
P1OUT |= 0x01; // Set P1.0 LED on
}
}
// ADC10 interrupt service routine
#pragma vector=ADC10_VECTOR
__interrupt void ADC10_ISR (void)
{
__bic_SR_register_on_exit(CPUOFF); // Clear CPUOFF bit from 0(SR)
}
#pragma vector=TIMER0_A0_VECTOR
__interrupt void ta0_isr(void)
{
TACTL = 0;
LPM0_EXIT; // Exit LPM0 on return
}