Other Parts Discussed in Thread: MSP430F149, MSP430G2553
书上写电源1.8~3.6V。锂电池充满电电压约有4.2V。求教。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: MSP430F149, MSP430G2553
书上写电源1.8~3.6V。锂电池充满电电压约有4.2V。求教。
楼主可以串二极管,硅管0.7左右。但是电流不同的时候,压降不一样,会造成MCU供电波动。
两个方法:
1、使用LDO,但是LDO的压降有最小值,所以不能充分利用锂电池的电量。
2、使用DCDC,电路比LDO负载,需要考虑EMI问题。但是能够充分利用电池能量,产品大多数是这样做。
Hi,Kelly,
最简单的办法就是加一个LDO,可靠稳定,如果希望效率高一些,如果需要连续的稳定电压,可将稳压值设定在3V,如果希望电源利用效率高一点3.3V,3.6V也可以,对于这种低功耗应用,最好不要使用DCDC。
电池容量是多大的?设计使用时间多长?
Regards,
Hardy