看到一个例程,上面讲:将SMCLK和MCLK配置为XT2跟配置为XT1的过程基本相同,唯一不同的是,在配置SMCLK和MCLK为XT2之前,需要将ACLK和REFCLK的时钟源配置好,因为ACLK和REFCLK的默认时钟源是XT1,而我们并没有配置启动XT1CLK,所以会产生XT1时钟错误,即XT1LFFG,因此,我们先将ACLK和REFCLK配置为芯片自带的时钟(REFOCLK或VLOCLK)或者即将启动的时钟XT2。
如果这样是对的,那么平时一些小程序根本就没有去设置过ACLK和REFCLK,难道也会出错?还是有哪个地方我没想到。希望可以解答一下,刚学430F5,很多地方都不太懂。