5529的系统时钟可以采用好几种方式,现在的问题是LAB实验里面采用的是不是XT2?我看程序的时候,程序配置的都是跟DCO相关的配置寄存器,因为里面的寄存器都是以DCO为前缀的,而我又问了下其他人,说DCOCLK是数字RC振荡器,频率比较低,而另外一个LFXT1也是低频的,在MSP430系列单片机资料上看到对DCO振荡器的说明,不是非常明白,外部LFXT1和XT2失效时,DCO振荡器就会自动使用为MCLK为系统提供时钟源,此时振荡器就会产生失效,触发NMI中断响应请求,也就是每个主程序文件里面都会有一个NMI的中断服务程序,将振荡器触发的失效标志清零,我这样理解不知道对不对???