This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我使用CCS5.4准备编译SimpliciTI-CCS-1.1.1中的CCTV30EM/Simple-Peer-to-Peer例程。
打开看到Properties-General-Compiler version 显示的是 TI3.2.1, Effective complier version 显示的是TI4.1.5
直接build可以通过,仅显示一个警告:This project was created using a version of compiler that is not currently installed: 3.2.1 [MSP430]. Another version of the compiler will be used during build: 4.1.5. Please install the compiler of the required version, or migrate the project to one of the available compiler versions by adjusting project properties.
但是只要我选择Compiler version为 TI 4.1.5,就再也改不回来了,而且编译直接出错。 Errors occurred during the build. Errors running builder 'CDT Builder' on project 'Project'. java.lang.NullPointerException 请问下这是什么情况?如何解决?
把工程文件夹里的Debug Release目录都删掉,删除之后,把工程clean一下再build呢?
如果还是不行,有一个解决办法就是新建一个工程,把原工程的源文件添加进去就OK了。
我做了如下工作:
1、卸载SimpliciTI整个软件包
2、将E:\workspace下面所有文件和文件夹全部删除
3、重新安装SimpliciTI软件包到D:\Texas Instruments
4、打开CCSv5.4,指定工作区路径到E:\workspace
5、Import project 路径为:D:\Texas Instruments\SimpliciTI-CCS-1.1.1\Projects\Examples\CC430EM\Simple_Peer_to_Peer
6、修改 compiler version 为TI V4.1.5
7、build projectt
然后就出现上述错误
并没有出现Debug或Release目录,只出现了\CC430F6137-LinkTo目录。
我用了CC4305137-LinkTo的模式,编译就正常,除了有如下的提示外。
This project was created using a version of compiler that is not currently installed: 3.2.1 [MSP430]. Another version of the compiler will be used during build: 4.1.5. Please install the compiler of the required version, or migrate the project to one of the available compiler versions by adjusting project properties.
此图示正常编译过的CC430F5137-LinkTo的Active Configure
此图是CC430F6137-LinkTo Active的工程编译,两者之间没有任何代码不同,工程设置也完全相同。唯一的区别是Compiler Version. 正常的是TI V3.2.1,错误的是TI V4.1.5
请教一下该怎么弄。