This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

从G2553移植模拟的I2C到F5438上



我在G2553上使用模拟I2C,一切正常,可以使用,尤其是主机接收从机应答部分的波形。但是把相同的程序移植到F5438以后,应答部分波形变得很奇怪。SCL自己先拉高,然后在SDA拉高前,SCL拉低。

但是正常主机接收从机应答,应该是

1.主机拉高SDA电平,然后释放SDA线。

2.SCL由低电平转为高电平并保持,然后读取SDA的电平。

3.若是从机应答,则这时SDA应被拉低。

4.然后SCL变为低电平。

5.最后SDA再被主机控制,并置为低电平。接收应答结束。

应该是按以上的步骤吧?可是换到F5438上就不是这样了,变成:SDA未拉高并释放。时钟就完成了应答时序。

下附我模拟I2C,检查从机的应答操作的程序。附图中上图是G2553的时序(正确),下图是F5438的时序。

试修改程序还是不行。求助各位专家啊啊啊

/*******************************************
函数名称:check
功 能:检查从机的应答操作
参 数:无
返回值 :从机是否有应答:1--有,0--无
********************************************/
void check(void)
{
uchar slaveack;


SDA_H;
_NOP(); _NOP();
SDA_in;
_NOP(); _NOP();
SCL_H;
_NOP(); _NOP();

slaveack = SDA_val; //读入SDA数值
while(slaveack)
{
slaveack = SDA_val;
}
SCL_L;
delay();

SDA_out;

}

一些宏定义

#define SCL_H P1OUT |= BIT7
#define SCL_L P1OUT &= ~BIT7
#define SDA_H P1OUT |= BIT6
#define SDA_L P1OUT &= ~BIT6
#define SDA_in P1DIR &= ~BIT6 //SDA改成输入模式
#define SDA_out P1DIR |= BIT6 //SDA变回输出模式
#define SDA_val P1IN&BIT6 //SDA的位值
#define SCL_out P1DIR |= BIT7
#define TRUE 1
#define FALSE 0