This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

如何解决430与5V其他单片机的通信问题??

Other Parts Discussed in Thread: SN74AVC1T45, TXB0101

如何解决430与5V其他单片机的通信问题??

想使用430单片机与现有的51单片机或PIC进行通信,如何解决电压不一致的问题?

  •  中间是可以加电平转换芯片的。

    请问你是什么接口?UART,I2C,SPI?

  • 你好!

    这个应用可分为4种情况考虑:

    1.5V输入到MSP430的I/O,标准方法加一个电平转换器,例如SN74AVC1T45,SN74LVC245,SN74LVC16245等,简单的方法加一个电阻限流即可,典型值10Kohm;

    2.MSP430的I/O输出驱动5V电平的I/O,标准方法加一个电平转换器,例如SN74AVC1T45,SN74LVC245,SN74LVC16245等,简单的方法,如果5V输入的I/O的VIH的最小值低于MSP430 I/O输出的VOH最小值(一般可视作MSP430的电源电压),则可串一个限流电阻直接驱动,反之,则可以用加三极管的方法驱动;

    3.5V I/O与MSP430 I/O双向同时通信,简单方法, 如果5V输入的I/O的VIH的最小值低于MSP430 I/O输出的VOH最小值(一般可视作MSP430的电源电压),则可串一个限流电阻直接驱动,如果不是,或者标准的方法,则是加一个方向自动识别的电压转化器,例如TXB0101等;

    4.如果是标准总线,例如IIC,SPI等则可选择专用总线电压和转换器,可以在这里查找:http://www.ti.com/lsds/ti/interface/application-specific-compact-flash-sd-mmc-i2c-products.page?paramCriteria=no

    Regards,

    Hardy

  • 你好,

    加电平转换芯片。