This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

液晶显示

Other Parts Discussed in Thread: MSP430F5529

现在正在用TI提供的开发板MSP430F5529,需要设计一个心电的实时采集与显示的系统,现在的方案是,利用定时器精确定时采样周期,心电的数据输出通过模拟量输出,用单片机的AD采样进行采集,然后将心电波形实时显示到液晶屏上,并将转换后的数据通过USB的方式发送给PC端。现在遇到的问题是实时性不够,就是液晶显示速度跟不上采集的速度,所以也会影响到发送到PC端的数据,我现在使用的是每采集到一个数据就反应到液晶上,波形会向左移动一个数据,也就是有数据时,就刷新液晶屏,重绘屏幕,这样子的效果是很低的,后来改进了一下,猜到2个或者3个数据就显示,但是这样的话,速度是快了,但是绘制出来的波形不连贯,跳跃性比较大,分析一下,慢的原因就是液晶绘制花时间比较长,但是不知道怎么改进???USB发送数据那部分有时候也会因为发送的数据量过大而跟主机断开,发送数据后返回的状态意思是bus is gone,这样就影响到数据的实时传送,USB底层协议我不是很了解,但是可不可以通过改动什么地方来优化USB传送数据这块???

  • 1. 你的心电数据的采样频率是多少?(ECG一般是1K,看你的是几导联的)

    2. MSP430F5529的ADC是12-BIT的,采样结果你是用12BIT还是转换成8BIT。姑且认为你是转换成8BIT。

    3. 液晶的接口是什么?并行口还是串行口,通信速率是多少? 液晶的点阵是多少?刷一次屏的时间是多少?

    4.  一般的ECG不会采用左移显示,而是从左到右刷新的方式,一次更新只刷新3-4列,波形到了最右边后又回到最左边显示最新波形,这样比较节约刷屏时间。

    5. 如果是1K的采样率,USB的数据不会太大,应该不存在USB断开的问题。