This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好!
在IAR5.3中的工程:按键中断检测可以正常工作,但是在CCS12中新建一个工程后,Build ALL 后进入DEBUG运行后,程序无法检测到按键中断。代码如下:
请问:IAR工程移植到CCS中是需要做哪些修改和注意点?
/***************************************************
程序功能:用中断方式读取四个独立式按键的键值,同时用
D1~D4四个LED的点亮来指示k1~K4四个按键的按下
----------------------------------------------------
测试说明:按动K1~k4四个按键,观察LED是否正确点亮
*******************************************************/
#include <msp430.h>
//#include <msp430x14x.h> //原IAR工程中使用的是这个头文件。
#include <msp430f149.h>
#define keyin (P1IN & 0x0f)
void delay(void);
typedef unsigned char uchar;
typedef unsigned int uint;
uchar KeyVal = 0; // 按键的键值
uchar i=0;
/********************主函数********************/
void main( void )
{
WDTCTL = WDTPW + WDTHOLD; //关闭看门狗
/*------选择系统主时钟为8MHz-------*/
BCSCTL1 &= ~XT2OFF; //打开XT2高频晶体振荡器
do
{
IFG1 &= ~OFIFG; //清除晶振失败标志
for (i = 0xFF; i > 0; i--); //等待8MHz晶体起振
}
while ((IFG1 & OFIFG)); //晶振失效标志仍然存在?
BCSCTL2 |= SELM_2 + SELS; //MCLK和SMCLK选择高频晶振
P1IES = 0x0f; // P1.0~P1.3选择下降沿中断
P1IE = 0x0f; // 打开中断使能
P1DIR &=~ (BIT0+BIT1+BIT2+BIT3); //设置P1.0~P1.3为输入状态
P4DIR = 0xff;
P4OUT = 0xff;
_EINT(); //打开全局中断控制位
while(1)
{
switch(KeyVal) //转换键值
{
case 1:
P4OUT&=~BIT0;KeyVal=0;break;
case 2:
P4OUT&=~BIT1;KeyVal=0;break;
case 3:
P4OUT&=~BIT2;KeyVal=0;break;
case 4:
P4OUT&=~BIT3;KeyVal=0;break;
default:break;
}
delay();
delay();
delay();
delay();
delay();
delay();
P4OUT = 0xff;
}
}
/*******************************************
函数名称:delay
功 能:用于消抖的延时
参 数:无
返回值 :无
********************************************/
void delay(void)
{
uint tmp;
for(tmp = 12000;tmp > 0;tmp--);
}
/*******************************************
函数名称:PORT1_ISR
功 能:P1端口的中断服务函数
参 数:无
返回值 :无
********************************************/
#pragma vector=PORT1_VECTOR
__interrupt void PORT1_ISR(void)
{
switch(P1IFG)
{
case 0x01:
if(keyin == 0x0e) //è?1?ê?μúò???°′?ü±?°′??
{
delay();
if(keyin == 0x0e)
{
while(keyin != 0x0f); //μè′y°′?ü·??a
KeyVal = 1;
P1IFG = 0;
break;
}
}
case 0x02:
if(keyin == 0x0d) //è?1?ê?μú?t??°′?ü±?°′??
{
delay();
if(keyin == 0x0d)
{
while(keyin != 0x0f); //μè′y°′?ü·??a
KeyVal = 2;
P1IFG = 0;
break;
}
}
case 0x04:
if(keyin == 0x0b)
{
delay();
if(keyin == 0x0b)
{
while(keyin != 0x0f);
KeyVal = 3;
P1IFG = 0;
break;
}
}
case 0x08:
if(keyin == 0x07)
{
delay();
if(keyin == 0x07)
{
while(keyin != 0x0f);
KeyVal = 4;
P1IFG = 0;
break;
}
}
default:P1IFG = 0;break;
}
}