Other Parts Discussed in Thread: MSP430FG6626, , MSP430FR6877
项目是用于小型手持PDA支付设备,之前对标的是LC88F83B0A,但是已经停产断货了,我按照推荐给到相应的型号为MSP430FG6626,但是经过对比,还是缺少两项功能。
项目需求如下:
- A display controller with at least a 64 x 16 matrix.
This may be possible with an external LCD / controller, but beware, the space on the board is very limited.
- 5 analog inputs for the flicker electronics
- A smartcard interface aka serial port with ISO7816-mode (this is not absolutely necessary).
- 5 I/O's for the smartcard interface
- one analog input for battery monitoring
- 8 normal I/O's for the keyboard.
- 3 timers
- Low power consumption! (we have only 2 CR2025 lithium batteries)
请问还有其他可以实现这些全部功能的型号吗