This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430FR6043: 声波风速测量,如何软件校准,校准的误差需要满足0.1m/s,

Part Number: MSP430FR6043


之前的对话:

之前向贵司提过问题,我们的工程师认为提供的风速和测试风速之间有一个比较明确的关系,接近1.2倍。如果L准确,则检查T12和T21测量值是否大于 20%。

顺便问一下,您可以接受软件校准吗? 软件校准后的误差是否可以接受?

请如何进行软件校准,只要最后的误差范围在0.1m/s,就行,我们产品就可以量产。