Part Number: MSP430AFE253
我的程序中如果把SD24GAINx 设定为0时。 计算公式是(AD值/7fff)*0.6V就可以正确算出具体的电压值。我现在的问题是想把这个-0.6V~0.6V这只范围缩少到一定的范围,是否可以修改SD24GAINx来达到效果?如果可以,我把SD24GAIN x设定为011即x8。计算公式(AD/7fff)*0.6中的0.6修改为多少?我尝试使用0.075是有偏差的,大概在0.0772才对。为何这样呢?是使用增益后出现的偏差吗?还是我这样理解就是错误的?