能否帮我看下这个官方例程?
|
这个例程可以开启25M的主时钟,但是我确实很多地方都看不懂啊,谁能帮我解释一下呢?主要是
void SetVcoreUp (unsigned int level)这个函数不懂,学1系列的时候,这里面的东西压根没见过,他们有什么作用?为什么要对他们进行设置?我试了其他可以开启25M的程序,结果发现,程序运行时他们都跑飞了,就这个程序可以开启。是不是
void SetVcoreUp (unsigned int level)可以防止跑飞啊?谢谢啊~ 程序如下: |
这个例程可以开启25M的主时钟,但是我确实很多地方都看不懂啊,谁能帮我解释一下呢?主要是
void SetVcoreUp (unsigned int level)这个函数不懂,学1系列的时候,这里面的东西压根没见过,他们有什么作用?为什么要对他们进行设置?我试了其他可以开启25M的程序,结果发现,程序运行时他们都跑飞了,就这个程序可以开启。是不是
void SetVcoreUp (unsigned int level)可以防止跑飞啊?谢谢啊~ 程序如下:
#include <msp430f5529.h>
void SetVcoreUp (unsigned int level)
{
// Open PMM registers for write
PMMCTL0_H = PMMPW_H;
// Set SVS/SVM high side new level
SVSMHCTL = SVSHE + SVSHRVL0 * level + SVMHE + SVSMHRRL0 * level;
// Set SVM low side to new level
SVSMLCTL = SVSLE + SVMLE + SVSMLRRL0 * level;
// Wait till SVM is settled
while ((PMMIFG & SVSMLDLYIFG) == 0);
// Clear already set flags
PMMIFG &= ~(SVMLVLRIFG + SVMLIFG);
// Set VCore to new level
PMMCTL0_L = PMMCOREV0 * level;
// Wait till new level reached
if ((PMMIFG & SVMLIFG))
while ((PMMIFG & SVMLVLRIFG) == 0);
// Set SVS/SVM low side to new level
SVSMLCTL = SVSLE + SVSLRVL0 * level + SVMLE + SVSMLRRL0 * level;
// Lock PMM registers for write access
PMMCTL0_H = 0x00;
}
void TIME(void)
{
SetVcoreUp (0x01);
SetVcoreUp (0x02);
SetVcoreUp (0x03);
UCSCTL3 = SELREF_2; // Set DCO FLL reference = REFO
UCSCTL4 |= SELA_2; // Set ACLK = REFO
__bis_SR_register(SCG0); // Disable the FLL control loop
UCSCTL0 = 0x0000; // Set lowest possible DCOx, MODx
UCSCTL1 = DCORSEL_7; // Select DCO range 50MHz operation
UCSCTL2 = FLLD_1 + 762; // Set DCO Multiplier for 25MHz
// (N + 1) * FLLRef = Fdco// (762 + 1) * 32768 = 25MHz // Set FLL Div = fDCOCLK/2
__bic_SR_register(SCG0); // Enable the FLL control loop
// Worst-case settling time for the DCO when the DCO range bits have been
// changed is n x 32 x 32 x f_MCLK / f_FLL_reference. See UCS chapter in 5xx
// UG for optimization.
// 32 x 32 x 25 MHz / 32,768 Hz ~ 780k MCLK cycles for DCO to settle
__delay_cycles(782000);
// Loop until XT1,XT2 & DCO stabilizes - In this case only DCO has to stabilize
do
{
UCSCTL7 &= ~(XT2OFFG + XT1LFOFFG + DCOFFG);
// Clear XT2,XT1,DCO fault flags
SFRIFG1 &= ~OFIFG; // Clear fault flags
}while (SFRIFG1&OFIFG); // Test oscillator fault flag
__no_operation(); //设断点观察时钟输出引脚上的波形和频率
// P3OUT|=BIT0;
}