This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

430能不能正常和长期工作在5V系统下?



我知道430是工作在3.3V的,但我的系统是5V的,我用430也可以工作,但我不知道它能否正常和长期的工作?

  • 真的?那这说明430还比较皮实^_^

    VCC到VSS的极限最大值是4.1V,超出这个范围厂家就无法保证芯片的可靠性,也很可能对芯片造成永久的损坏,你当前看不出有问题,或许运行一段时间就会出现问题了。所以如果你是做产品,还是别这么用的好,否则后患很可怕。

    我曾遇到不小心将将近8V的电压加到电源引脚上的情况,结果片子就坏了。

  • 最好是在Datasheet推荐的电压范围以内工作,不然将会出现不可预见的问题。

    可以加个LDO降下压。