您好:
看TI官网有关MSP430FR573X系列FRAM 读写速度的资料,
得知,
写的速度,通过配置,是可以超过8MHz的,
请问读的速度可以超过8MHz吗?
如果能,写的最大的速率应该是多少?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好:
看TI官网有关MSP430FR573X系列FRAM 读写速度的资料,
得知,
写的速度,通过配置,是可以超过8MHz的,
请问读的速度可以超过8MHz吗?
如果能,写的最大的速率应该是多少?
The embedded FRAM on MSP430 devices can be accessed (read or write) at a maximum speed of
8 MHz. Above 8 MHz, wait states are used when accessing FRAM. Typical write speeds can exceed
2 MBps with FRAM compared to approximately 14 kBps on Flash devices
可以在这里查看www.ti.com/.../slaa526.pdf