Other Parts Discussed in Thread: MSP430G2231
关于ADC10与低功耗的问题
msp430G2系列
手册中写道:
WhenREFON=1,but no conversionis active,the bufferis automatically disabled and automatically
re-enabled when needed.When the bufferis disabled,it consumes no current.In this case,the band-gap
voltage sourcere mains enabled.
请问在框图中是通过哪里控制的呢?
When REFOUT=1,the REFBURST bit controls the operation of the internal reference buffer.When
REFBURST=0,the buffer will be oncontinuously,allowing the reference voltage to be present outside
the device continuously.When REFBURST=1,the bufferis automatically disabled when the ADC10 is
not actively converting,and automatically re-enabled when needed.
请问REFBURST 是否只对输出有影响?对buffer无影响?前一段是否有个条件就是 REFOUT不等于1或者 REFOUT=1但是
REFBURST=1?
自带的时钟振荡器稳定时间是多少?也就是核心的建立时间tADC10ON一般为100ns?
REF的稳定时间在低功耗设计时如何考虑?长了不好,短了不行,用什么计时?
The ADC10is designed for low power applications.When the ADC10 is not actively converting,the core is
automatically disabled and automatically re-enabled when needed.The ADC10OSC is also automatically
enabled when needed and disabled when not needed.When the core or oscillatoris disabled,it
consumes no current.这个和ADC10ON控制位是什么关系?还有ADC10ON内置的振荡器不如果不用用其它时钟源是否能减低
功耗?手册中没有内置振荡器的功耗数据。
ADC10的功耗和时钟源频率的高低在低功耗要求下如何权衡?
对于如果考虑到尽量减低功耗,msp430需要在哪些方面注意到?有没有详细的考虑到各种情况的指导手册?官方有个中文
视频,讲到了低功耗的注意事项,感觉太短了,也许应该考虑的都讲到了,其它的没有必要考虑,但是作为初学者,即使
不用考虑,有时候还是有疑问需要给个确定的回答。例如,定时器本身也有没有功耗?和频率有没有关系?其它的模块呢
?
能不能就低功耗问题给点参考?谢谢!