This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430F169

Other Parts Discussed in Thread: MSP430F169

MSP430F169内置的12位DAC能发出50-80khz的线性调频信号吗,芯片资料没有说明DAC的转换速率,还有内置的DAC的驱动能力咋样啊 ,能直接驱动内阻为8欧姆的陶瓷片吗?

  • Liewei Deng,

    MSP430F169 datasheet中提到DAC12 load current 在供电为3V时,最大为1mA.

    一般DAC使用,可以和DMA结合起来,以达到快速输出。dasheet中提到最最大full-scale settling time为200us (与DAC12AMPx设置有关),你可以按照你的设置瓶罐一下,一个周期内输出几个点,看看够不够。

    希望对你有帮助!O(∩_∩)O~