问题详细描述:(1)首先配置P1SEL|=BIT0,即声明P1.0将用作TA0CLK。
(2)我的main函数里面有一个while(1)循环,里面有三个中断、一些LED指示灯(会闪烁)以及LCD显示程序;当正常启动且P1.0不外接信号时,屏幕显示正常LED指示灯正常。
(3)在正常显示情况下,突然在P1.0加上信号,就会发现显示屏没有显示,LED指示灯不再正常变化;
(4)先在P1.0加信号,再启动开发板,会发现程序貌似根本没有进入while函数.
(5)所加信号为1MHZ,峰峰值6V的方波。
是我的P1.0配置不对,还是我的TA0里面配置不对,还是其它什么原因。还有,TI有没有这方面的例程