This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
请问一下,在供电为3.3时,管腿的输出约为3V,那么电流为多少?
BETTER ZHU,
请问用的是哪个device?
对应的datasheet上均有具体数据。一般默认情况下,当Vcc=3V时,IO最大可提供6mA电流,但所有IO总电流不能超过48mA.
MSP430F5xxx/6xxx有IO强驱动能力(Full Drive Strength),可以使能,每个IO可提供15mA左右的电流。
希望对你有帮助!O(∩_∩)O~
BR,
Lina
楼上回答的不错
如果I/O输出不小心与地短路,短路电流也是6mA吗?会不会造成I/O管脚的损坏或整个芯片的损坏?
还有一个问题是如果我两个输出的管脚不小心短路了,这样两个管脚流过的电流是怎么算?会不会造成损坏?
谢谢