This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

向TI的技术专家及广大网友咨询一个关于MSP430F6436ADC转换的问题:急~!很急~!甚急~!求救~!

Other Parts Discussed in Thread: MSP430F6436

我们公司正在做一个小项目:项目产品的功能、规格及问题点描述如下。

产品功能:采用MSP430F6436处理器,制作三个压电触摸按键,按键的材料是一种具有压电效应的压电薄膜(即对压电薄膜施加一定压力时,薄膜产生扭曲形变,随即产生电荷,电荷经电荷放大器放大后,转换为电压;不施加压力时,处于静态状态,无任何电荷、电量、电压产生),三个按键连接MSP430F6436的三个不同ADC输入引脚,在任意时刻按下某个按键时,显示出该按键的压力大小数据。

实现方法:采取轮询ADC输入口的方式,即,在某一时刻,只有一个按键所对应的ADC输入引脚有效,其他按键所对应的ADC输入引脚无效。ADC的采样转换方法为单通道单次采样。具体控制过程描述:当MSP430F6436轮询到某一个ADC输入引脚时,首先对ADC输入引脚进行切换,然后采用单通道单次采样对该ADC输入通道采样一次,采样时,main函数等待ADC中断服务程序完成,待完成之后,main函数再往下执行,采样完成后对采样数据和1000进行比较(因为有点工频干扰,所以设置了1000的门限值),如采样值大于等于1000,则进行5毫秒的延时消抖处理,5毫秒延时之后,接着再采用单通道单次采样对该ADC输入通道采样一次,若采样值还是大于等于1000,则认为是“有键按下”,紧接着对该ADC输入通道进行多次采样,采样率为5毫秒的单通道单次采样,直至所采集到的数据跌落至1000以下,采样期间,main函数等待ADC中断服务程序完成,待完成之后,main函数再往下执行;最后从多次采样到的数据中找出最大值,并转换为压力大小显示出来,最后一步,将ADC输入通道切换到下一通道。 三个ADC输入通道均按此方式进行处理,轮回循环。

问题点: 1、当从A键输入通道切换到B键输入通道时,而此时此刻不触按B键,但B键所对应的ADC输入通道却能采集到一个很大的数据,应经超出了1000的门限值,最大时有2000多的值;理论上讲,当B键没有任何触按时,除了工频干扰外,是没有其他信号输入的。从B键切换到C键时,C键也出现这样的情况。 2、执行ADC12_A_startConversion(ADC12_A_BASE, ADC12_A_MEMORY_0,ADC12_A_SINGLECHANNEL)这个函数时,会产生一个脉冲信号;该脉冲信号可以传输到相应的ADC输入引脚外面,该脉冲信号是否会影响ADC的采样值,脉冲信号是否作为ADC输入信号的一部分? 3、我原以为是通道轮询切换的问题,后来我采用了序列通道采样方式,问题更严重,在不对任何键按下时,ADC采样到的数据更是离谱。

烦请TI的技术专家及广大网友提供帮助,谢谢~!附件是该项目的软件架构框图。

力度按键软件架构框图.pdf