This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

【分享】eZ430-Chronos使用心得



eZ430-Chronos到手也有几天了,一直没好好地发表帖子。

本来准备十一假期好好玩玩,但7天假期除去三天上班,然后出去陪媳妇的时间,发现比平时还要忙。

经过购买和几天的使用,有以下体会和思路:

1、关于物流:联邦快递在海外的路途很给力,周五购买的eZ430-Chronos,周日就跨越太平洋到达北京了。周一过的海关。然后周二就是显示客户无法找到。于是周三一早我就和联邦快递的客服联系,提供了中文的地址。周三周四任然显示客户无法找到。直到周五才收到货物。在国内花费了5天时间,联邦快递在国内不给力啊,还赶不上国内的物流。

2、关于eZ430-Chronos的功能:

1)年月显示是西方格式,不太符合中国人的习惯。这个可能和设计者的习惯有关。不过问题不大,可以自己改下程序。

2)闹铃的声音,比较小。这个貌似和手表的低功耗有关,声音大了功耗就会比较高。没有太好的办法~~

3)心率计模式,需要外置心率计。搜了搜发现TI的心率计好贵,其他的心率计没找到支持433频率传输的,这个功能有点鸡肋,后续准备编程去掉这个工作模式,或者改成其他功能。

4)eZ430-Chronos有一个功能是两个eZ430-Chronos间通讯,因为手里只有一个eZ430-Chronos,所以这个功能没办法实验,不知道能通讯什么数据。但可以考虑交换名片。现在的名片各种各样,有用手机交换图片版的名片,为什么不能用eZ430-Chronos来交换名片数据呢?当然,图片版的名片肯定是存储不下的,不过可以存放姓名、电话、工作单位、职位等信息,应该问题不大。回头去研究下eZ430-Chronos还有多大空闲存储空间。相信这会是一个比较炫的应用。