Other Parts Discussed in Thread: MSP430F5438A
芯片用MSP430F5438A,程序下载到板子后,一直在_data 16_memzero里死循环。网上查了下,可能是因为初始化变量时有大数组,导致看门狗不断复位,这个初始化的过程在进入main函数之前,解决方法有:
1、对数组用__no init_定义;
2、修改IAR中的Cstartup.s43文件中的__program_start子程序,增加一个关闭看门狗的设置
问题:1、__no init_如何使用?例如数组unsigned char ABCbuffer[500]; 如何用__no init_定义?
2、在Cstartup.s43中__program_start关于看门狗的代码如下,在哪儿添加关闭WDT?
__program_start:
PUBLIC ?cstart_begin ?cstart_begin:
// -------------------- // Turn off the watchdog. //
// Note: This is excluded by default. Please define
// DISABLE_WATCHDOG to include it. //
#ifdef DISABLE_WATCHDOG
MOV #WDTPW + WDTHOLD, &WDTCTL
#endif