This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

5438A益出的问题

 67 906 bytes of CODE  memory

  5 295 bytes of DATA  memory (+ 181 absolute )

 14 816 bytes of CONST memory

现象就是能DEBUG,但是就是一直停在data16——memero里面,

这样怎么就溢出了的,不是16K的吗?堆栈我设置是:160、160、80 ,即使设置再大也没什么用。

如果RAM的数组改小一点,就可以了。

编译后是:

 68 386 bytes of CODE  memory

  4 295 bytes of DATA  memory (+ 181 absolute )

 14 816 bytes of CONST memory

这样就没任何问题。

我想问一下这个是否就是这样了,这是不是真的16K的反映啊。