This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

大家看一下这是不是CCS4的BUG,第254行的语句编译出来的结果明显不对!



版本信息如下:

Code Composer Studio

Version: 4.2.1.00004

源程序如下:

#pragma vector=PORT2_VECTOR

__interrupt void Port2ISR()

{  

//    volatile unsigned char temp;

   P2IFG &= ~BIT1;

//    temp = P2IN & BIT2;

   if(P2IN & BIT2 == BIT2)

   {

       key_encode_value = 0x1a;

   }

   else

   {

       key_encode_value = 0x1b;

   }

}

编译结果如下

0xE1A6:   12B0 E1DC           CALL    #abort

243         P2IFG &= ~BIT1;

       Port2ISR:

0xE1AA:   C3E2 002B           BIC.B   #2,&Port_1_2_P2IFG

245         if(P2IN & BIT2 == BIT2)

0xE1AE:   B3D2 0028           BIT.B   #1,&Port_1_2_P2IN

0xE1B2:   2004                JNE     (C$L12)

251             key_encode_value = 0x1b;

0xE1B4:   40F2 001B 0208      MOV.B   #0x001b,&key_encode_value

0xE1BA:   1300                RETI

247             key_encode_value = 0x1a;

       C$L12:

0xE1BC:   40F2 001A 0208      MOV.B   #0x001a,&key_encode_value

253     }

0xE1C2:   1300                RETI

加了一个临时变量缓存一下结果就对了,程序如下:

#pragma vector=PORT2_VECTOR

__interrupt void Port2ISR()

{  

   volatile unsigned char temp;

   P2IFG &= ~BIT1;

   temp = P2IN & BIT2;

   if(temp == BIT2)

   {

       key_encode_value = 0x1a;

   }

   else

   {

       key_encode_value = 0x1b;

   }

}

编译结果:

       Port2ISR:

0xE110:   120F                PUSH    R15

0xE112:   8321                DECD.W  SP

243         P2IFG &= ~BIT1;

0xE114:   C3E2 002B           BIC.B   #2,&Port_1_2_P2IFG

244         temp = P2IN & BIT2;

0xE118:   422F                MOV.W   #4,R15

0xE11A:   F25F 0028           AND.B   &Port_1_2_P2IN,R15

0xE11E:   4FC1 0000           MOV.B   R15,0x0000(SP)

245         if(temp == BIT2)

0xE122:   92E1 0000           CMP.B   #4,0x0000(SP)

0xE126:   2404                JEQ     (C$L12)

251             key_encode_value = 0x1b;

0xE128:   40F2 001B 0208      MOV.B   #0x001b,&key_encode_value

0xE12E:   3C03                JMP     (C$L13)

247             key_encode_value = 0x1a;

       C$L12:

0xE130:   40F2 001A 0208      MOV.B   #0x001a,&key_encode_value

253     }

       C$L13:

0xE136:   5321                INCD.W  SP

0xE138:   413F                POP.W   R15

0xE13A:   1300                RETI