This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430F6733的SD24_B采样AD获取的电压值与实际不符!是我哪里错了吗?

Other Parts Discussed in Thread: MSP430F6733

芯片MSP430F6733,使用外部基准电压3.0V,过采样OSR=256,精度24位

我外部输入电压0.61V时, 经过SD24_B转换后获取的数据除以0x1000000,再乘以3.0,结果居然有1.83伏左右

我外部输入电压0.88V时, 经过SD24_B转换后获取的数据除以0x1000000,再乘以3.0,结果居然有1.97伏左右

我有点搞不懂了,请帮忙分析下是怎么回事

下面是我的采样代码:

 

unsigned long resultsVoltages[10];

unsigned long baseVoltages[10];

unsigned char voltageIndex;

float results,bases;

 

void main()

{

   SD24BCTL0 =  SD24SSEL_1;

   SD24BCCTL1 = SD24SNGL | SD24SCS_4;      // Single conversion, group 0

   SD24BCCTL2 = SD24SNGL | SD24SCS_4;      // Single conversion, group 0

   SD24BIE = SD24IE2;                      // Enable channel 2 interrupt

   delay_ms(10);

   voltageIndex=0;

  

   while(voltageIndex<10)

   {

      SD24BCTL1 |= SD24GRP0SC;                // Set bit to start conversion

     __bis_SR_register(LPM0_bits | GIE);     // Enter LPM0 w/ interrupts

     SD24BCTL1 &= ~SD24GRP0SC;               // Clear bit for next conversion

     __no_operation();                       // SET BREAKPOINT HERE

     voltageIndex++;

   }

  results=0;

   for(int i=0;i<10;i++)

   {

     results+=resultsVoltages[i];

   }  

   results/=10;

   results=results*3.0/0x1000000;

   floatToStr(results,s,5);  

   displayFloat(results);

   bases=0;

   for(int i=0;i<10;i++)

   {

     bases+=baseVoltages[i];

   }

   bases/=10;

   bases=bases*3.0/0x1000000;

   displayFloat(bases);

   delay_ms(2000);

}

 

 

#pragma vector=SD24B_VECTOR

__interrupt void SD24BISR(void)

 {   

   switch (SD24BIV)    

{

         case SD24BIV_SD24OVIFG:                     // SD24MEM Overflow

             break;

         case SD24BIV_SD24TRGIFG:                    // SD24 Trigger IFG

             break;

         case SD24BIV_SD24IFG0:                      // SD24MEM0 IFG

             break;

         case SD24BIV_SD24IFG1:                      // SD24MEM1 IFG

             break;

         case SD24BIV_SD24IFG2:                      // SD24MEM2 IFG

             resultsVoltages[voltageIndex] = SD24BMEMH1;                   // Save CH2 results (clears IFG)

             resultsVoltages[voltageIndex] = (resultsVoltages[voltageIndex] << 16) | SD24BMEML1; // Concatenate lower and upper words

             baseVoltages[voltageIndex]  = SD24BMEMH2;

             baseVoltages[voltageIndex] = (baseVoltages[voltageIndex] << 16) | SD24BMEML2;

             break;     }

    __bic_SR_register_on_exit(LPM0_bits);           // Exit LPM0

 }