This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430 5438 LCD顯示問題

Other Parts Discussed in Thread: MSP430F5438, MSP430F5438A

請問MSP430 5438晶片,我溫度感測在電腦上讀來的時事正確的,請問要如何用LCD讀出我電腦上的溫度,有沒有範例可以參考,謝謝!

  • 你要自己写液晶驱动程序,虽然开发板已经写了部分,但是不一定适合你的。所以你还要在看看液晶的例程,然后再编写适合自己的程序。

  • 你好!

    MSP430F5438或者MSP430F5438A均没有段式LCD驱动器,如果要驱动液晶有两个方法,一是外部加一颗LCD驱动器,MCU将数据传输到外部LCD驱动器,再点LCD。

    还有一种是用IO模拟LCD driver,硬件和软件上稍显复杂。

  • 最好还是先用外部LCD驱动器,比如HT1620这种,使用起来也比较方便。后期需要优化硬件,降低成本再做IO口模拟LCD驱动器的方案。

  • 可以提供一下你使用的LCD的型号吗?

    如果是1602和12864之类的网上有很多参考例程,移植一下就可以支持了,这个还是蛮简单的。如果是其他的,因为没有那么常见的话你可能还需要看一下LCD的说明说,或者在网络上再找一下。