各位:刚学MSP430,我是用MSP430F2132的芯片,该款芯片好像不支持USART Peripheral Interface, UART Mode 是吗?因为我编程时写:U0CTL=ox01;编译就出错,说U0CTL没定义。谢谢指点!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
各位:刚学MSP430,我是用MSP430F2132的芯片,该款芯片好像不支持USART Peripheral Interface, UART Mode 是吗?因为我编程时写:U0CTL=ox01;编译就出错,说U0CTL没定义。谢谢指点!
//******************************************************************************
// MSP430F21x2 Demo - USCI_A0, UART 19200 Echo ISR, HF XTAL SMCLK
//
// Description: This program will echo a received character, RX interrupt
// service used. XT1 oscillator used in this example.
// ACLK = MCLK = SMCLK = BRCLK = LFXT1CLK = 8MHz
// Baud rate divider with 8MHz XTAL @19200 = 8MHz/19200 = ~416.6
// //* An external 8MHz XTAL on XIN XOUT is required for LFXT1CLK *//
//
// MSP430F21x2
// -----------------
// /|\| XIN|-
// | | | 8MHz
// --|RST XOUT|-
// | |
// | P3.4/UCA0TXD|------------>
// | | 19200 - 8N1
// | P3.5/UCA0RXD|<------------
//
// A. Dannenberg
// Texas Instruments Inc.
// January 2007
// Built with CCE Version: 3.2.0 and IAR Embedded Workbench Version: 3.41A
//******************************************************************************
#include "msp430x21x2.h"
volatile unsigned int i;
void main(void)
{
WDTCTL = WDTPW + WDTHOLD; // Stop WDT
BCSCTL1 |= XTS; // ACLK = LFXT1 = HF XTAL
BCSCTL3 |= LFXT1S1; // 3 ?16MHz crystal or resonator
do
{
IFG1 &= ~OFIFG; // Clear OSCFault flag
for (i = 0xFF; i > 0; i--); // Time for flag to set
}
while (IFG1 & OFIFG); // OSCFault flag still set?
BCSCTL2 |= SELM_3 + SELS; // MCLK = SMCLK = LFXT1 (safe)
P3SEL = 0x30; // P3.4,5 = USCI_A0 TXD/RXD
UCA0CTL1 |= UCSSEL_2; // SMCLK
UCA0BR0 = 160; // 8MHz/19200 = ~416.6
UCA0BR1 = 1; //
UCA0MCTL = UCBRS2 + UCBRS1; // Modulation UCBRSx = 6
UCA0CTL1 &= ~UCSWRST; // **Initialize USCI state machine**
IE2 |= UCA0RXIE; // Enable USCI_A0 RX interrupt
__bis_SR_register(LPM0_bits + GIE); // Enter LPM0, interrupts enabled
}
// Echo back RXed character, confirm TX buffer is ready first
#pragma vector=USCIAB0RX_VECTOR
__interrupt void USCI0RX_ISR(void)
{
while (!(IFG2 & UCA0TXIFG)); // USCI_A0 TX buffer ready?
UCA0TXBUF = UCA0RXBUF; // TX -> RXed character
}
发一个demo程序基于F21X2的,U0CTL应该是UCA0CTLx之类的