我用的是MSP430F2274,在程序初始化的时候配置了IO中断P1.0和P1.1,还有ADC10通道0-5,在单片机休眠的时候进不了IO中断,可是在休眠之前再次配置IO中断的话就可以进入IO中断,IO中断是配置上拉下降沿触发中断的,在单片机运行的时候仿真一切功能正常,就是在休眠的时候唤醒不Leeds
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我用的是MSP430F2274,在程序初始化的时候配置了IO中断P1.0和P1.1,还有ADC10通道0-5,在单片机休眠的时候进不了IO中断,可是在休眠之前再次配置IO中断的话就可以进入IO中断,IO中断是配置上拉下降沿触发中断的,在单片机运行的时候仿真一切功能正常,就是在休眠的时候唤醒不Leeds
你把如下的例程测试下
void main(void) {
WDTCTL = WDTPW + WDTHOLD; // Stop watchdog timer
P1IE |= 0x03; // P1.0 P1.1 interrupt enabled
P1IES |= 0x03; // P1.0,P1.1 Hi/lo edge
P1IFG &= ~0x03; // P1.0,P1.1 IFG cleared
_BIS_SR(LPM4_bits + GIE); // Enter LPM4 w/interrupt }
// Port 1 interrupt service routine
#pragma vector=PORT1_VECTOR
__interrupt void Port_1(void)
{
P1IFG &= ~0x03; // P1.0,P1.1 IFG cleared
}
测试了上面的IO中断功能都没有错,可以进入中断,我自己写的函数把IO中断初始化放在休眠之前也可以中断,就是放在程序最开始的地方不能进入中断
测试了上面的IO中断功能都没有错,可以进入中断,我自己写的函数把IO中断初始化放在休眠之前也可以中断,就是放在程序最开始的地方不能进入中断