L092怎么编程,FET430是3.3V的啊.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
MSP-FET430UIF 软件课配置电压范围,我记得是可以配置1.8V-3.6V的,具体你查下软件的使用说明
FET430UIF 具有电源管理功能,设置的电压范围是:1.8V~3.6V
可以右击工程名 option>FET Debugger的 Target VCC进行设置