数据手册中有两个对CCR0的描述 看管脚定义 第一张图片表格的注释似乎是对的
请TI工程师帮忙核对一下
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
感谢您的提问!
我检查了一下datasheet中的内容:
7.1 Pin Diagrams
7.2 Pin Attributes
Figure 9-2. TA0 and TA1 Signal Connections
Figure 9-3. TA2, TA3 and TB0 Signal Connections
以下是我认为在不同timer_A上CCRx连接到外部引脚的情况:
TA0: CCR1 and CCR2
TA1: CCR1 and CCR2
TA2: CCR0, CCR1 and CCR2
TA3: CCR0, CCR1 and CCR2