This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430G2553 (LaunchPAD)供电问题

Other Parts Discussed in Thread: CC1101

HI

     我遇到一个比较诡异的问题,如果用USB->TTL 芯片 连接G2553的P1.1, P1.2, GND,无论是否给VCC供电,系统均能正常工作。

此时串口工作正常。

      但是如果连接CC1101后,不给430的VCC供电,射频的接收距离为50m,给VCC供电,射频接收距离为25米,降低了50%。

哪位大哥可以给点意见。

  • 请问你 USB转TTL 5V的还是3.3V的

  • 你这是两个问题 1.把TTL电平连接到MSP430的管脚上,不给VCC供电,MSP430照样工作 因为MSP430的管脚都连有上拉到VCC,当管脚出现高电平的时候,会通过上拉电阻给VCC供电,上拉电阻大概为35K,所以如果系统功耗很低的情况下,给GPIO电平也会让CPU工作起来。但这样的风险很大,容易造成管脚损坏 3. 系统供电时,造成了CC101的接收距离降低 这个可能是由于电磁干扰造成的,你的CC1101板要距离LAUNCHPAD的电源远一点,忒别是天线要远离电源,如果可能,在CC1101上加屏蔽罩.