This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

msp430f149 iar5.2

Other Parts Discussed in Thread: MSP430F149

#include "msp430f149.h"
#include "my.h"

#define  Number_of_Results   5
unsigned int results[Number_of_Results];
unsigned int average = 0;
unsigned char nADC_Flag = 0 ;
void main()
{
  unsigned char  i=0;
  unsigned char buffer[6];
  buffer[5] = '\0';
  WDTCTL = WDTPW + WDTHOLD;
  _DINT();
  Init_CLK();  
  Init_ADC();
  Init_TimerA();
  Init_UART();
  _EINT();
 

  for(;;)
  {
    if(nADC_Flag==1)
    {
      nADC_Flag = 0 ;
      Trans_val(average,buffer);
      buffer[4]=0x3b-0x30;
      buffer[3]= buffer[2];
      buffer[2] = buffer[1];
      buffer[1] = '.'-0x30;
      for(i = 0; i < 4; i++)
      buffer[i] += 0x30;
      PutString(buffer);  
    }
  }
}

void Init_CLK(void)
{
  unsigned char i;
  //将寄存器的内容清零
  //XT2振荡器开启
  //LFTX1工作在低频模式
  //ACLK的分频因子为1
  BCSCTL1 = 0x00;
  do
    {
      //清除标志
      IFG1 &= ~OFIFG;
      for( i = 0x3f ; i>0; i--);
    }while((IFG1 & OFIFG)!=0 );
  BCSCTL2 = 0x00;
  //MCLK的时钟源为8MHZ,分频因子默认为1.
  BCSCTL2 += SELM_2 + DIVM_1;
  //SMCLK的时钟源为8MHZ,分频因子默认为1.
  BCSCTL2 += SELS + DIVS_1 ;
}

void Init_ADC(void)
{
    //设置P6.0为模拟输入通道
    P6SEL = 0x01;
    //设置ENC为0,从而修改ADC12寄存器的值
    ADC12CTL0  &=  ~(ENC);
    //转换的起始地址为:ADCMEM0
    ADC12CTL1 |= CSTARTADD_0;
    //选择通道为A0
    ADC12MCTL0 = INCH_0;
    //5  单通道单次转换
    ADC12CTL1 |= CONSEQ_0;
    //时钟源为SMCLK
    ADC12CTL1 |= ADC12SSEL_3;
    //ADC时钟源分频
    ADC12CTL1 |= ADC12DIV_7;
    ADC12CTL1 |= SHP;
     //打开ADC12内核
    ADC12CTL0 |= ADC12ON;
     //使能ADC
    ADC12CTL0 |= ENC;
}


void Init_TimerA(void)
{
  TACTL = SSEL1 + TACLR;
  TACTL += ID1;
  TACTL += ID0;
  //CCR0允许中断
  CCTL0 = CCIE;
  //频率为250HZ;
  CCR0 = 4000;
  //计数模式
  TACTL |= MC0;
}

#pragma vector=TIMERA0_VECTOR
__interrupt void Timer_A(void)
{
    static int index = 0;
    ADC12CTL0 &= ~ENC;
    results[index++] = ADC12MEM0;
    if(index == Number_of_Results)
    {
     unsigned char i = 0;
     for(i = 0 ; i < Number_of_Results ; i++)
       {
         average +=results[i];
       }
     average >>= 5 ;
    index = 0;
    nADC_Flag = 1;
   }
  ADC12CTL0 |= ENC ;
}


void Init_UART(void)
{
    P3SEL |= 0x30;                            // P3.4,5 = USART0 TXD/RXD
    ME1 |= URXE0 + UTXE0;                             // Enable USART0 T/RXD
    UCTL0 |= CHAR;                            // 8-bit character
    UTCTL0 |= SSEL1;                          // UCLK = SMCLK
    UBR00 = 0x1A;                             //   38400   32k/9600 - 3.41
    UBR10 = 0x00;                             //
    UMCTL0 = 0x00;                            // Modulation
    UCTL0 &= ~SWRST;                          // Initialize USART state machine
}
void Send1Char(unsigned char sendchar)
{
      while (!(IFG1 & UTXIFG0));    //等待发送寄存器为空        
      TXBUF0 = sendchar;
  
}
void PutString0(unsigned char *ptr)
{
      while(*ptr != '\0')
      {
            Send1Char(*ptr++);                     // 发送数据
      }
}
void PutString(unsigned char*ptr)
{
      while(*ptr != '\0')
      {
            Send1Char(*ptr++);                     // 发送数据
      }
      while (!(IFG1 & UTXIFG0));
                                 //发送换行指令
}

void Trans_val( unsigned int Hex_Val, unsigned char *ptr)
{
    unsigned long caltmp;
    unsigned Curr_Volt;
    unsigned t1;
   
    caltmp = Hex_Val;
    caltmp = (caltmp << 5) + Hex_Val;           //caltmp = Hex_Val * 33
    caltmp = (caltmp << 3) + (caltmp << 1);     //caltmp = caltmp * 10
    Curr_Volt = caltmp >> 12;                   //Curr_Volt = caltmp / 2^n
    ptr[0] = Curr_Volt / 100;                   //Hex->Dec变换
    t1 = Curr_Volt - (ptr[0] * 100);
    ptr[1] = t1 / 10;
    ptr[2] = t1 - (ptr[1] * 10);
    return;
}