添加至 MSP430F2370频率总是 wiki 页面

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430F2370频率总是



请问在MSP430F的MCU在采用片内振荡器或外部有源晶振时,能否在XOUT脚上测到波形?

另外在将XOUT管脚用作IO口时(P2SEL &= ~BIT7),为什会引起外部时钟失效?(OFIFG 始终为1,清不了0)

  • 内部振荡和外部有源晶振在XOUT是测不到波形。XOUT失效的问题是时钟配置问题,在msp430 user guider有一句对有源晶振的说明:In bypass mode of operation, XIN can accept an external clock

    input signal and XOUT is configured as a general-purpose I/O. The PSEL bit associated with XOUT is a

    don't care.

  • 我试了,不论把POWER_PIN 和POWER_ON 加到do while循环前面或是后面,如果没有P2SEL &= ~BIT7 这句, P2,7(XOUT)脚都没有输出. 如果加上,则无论在什么地址, OFIFG则始终置1,软件无法清除的.

    程序如下:

    #define POWER_PIN  P2SEL &= ~BIT7;P2DIR |= BIT7;

    #define POWER_ON   P2OUT |= BIT7;

    #define POWER_OFF  P2OUT &= ~BIT7;

    #define ENABLE_SET  P1DIR |= BIT0  // P1.0 ist switched in output direction

    #define TRF_ENABLE  P1OUT |= BIT0  // EN pin on the TRF796x

    #define TRF_DISABLE  P1OUT &= ~BIT0

    viod main(viod)

    {

    unsigned char ii1 = 0;

    WDTCTL = WDTPW + WDTHOLD;

    POWER_PIN;                   //如果加上这句,则程序一直在DO循环里出不来,取消这句则一切正常。

    POWER_ON;

    ENABLE_SET;

    TRF_ENABLE;

        BCSCTL1 |= XTS + XT2OFF;               // ACLK = LFXT1 HF XTAL

           BCSCTL3 |= LFXT1S1;                                        // turn external oscillator on

         while ((IFG1 & OFIFG) == OFIFG)

            IFG1 &= ~OFIFG;

        do

        {

           IFG1 &= ~OFIFG;                     // Clear OSCFault flag

           for (ii1 = 0xFF; ii1 > 0; ii1--)   // Time delay for flag to set

           {

           }

        } while ((IFG1 & OFIFG) == OFIFG);      // OSCFault flag still set?  如果XOUT用作IO口时,程序一直在里面,OFIFG位一直为1

        BCSCTL2 |= SELM1 + SELM0 + SELS;      // MCLK = SMCLK = HF LFXT1 (safe)

    while(1);

    }

  • 寄存器配置上需要做些修改.

    有源晶振和晶体(crystal)在寄存器的设置上是不一样的.

    使用有源晶振的时候,需要把XT1关掉.否则OFIFG会置位

    "BCSCTL3 |= LFXT1S1; " 应该改为    BCSCTL3 |= LFXT1S_3"

    还要加一句话 " __bis_SR_register(OSCOFF);"

    试试看

  • 您好,

    在User's Guide 277页中有这么一句“LFXT1 may be used with an external clock signal on the XIN pin in either LF or HF mode when LFXT1Sx = 11, OSCOFF = 0 and XCAPx = 00,”

    也就是说如果使用外部时钟信号,寄存器的相应位做如下设置:XTS = 0,LFXT1Sx = 11, OSCOFF = 0 ,XCAPx = 00

    POWER_PIN也应当设置。