This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ccs中 G2553.串口接受中断,为何进不去?,通过上位机调试也无法进入,求解释。



中断程序

void CH376_PORT_INIT( void ) /* 由于使用异步串口读写时序,所以进行初始化 */
{
DCOCTL = 0; // Select lowest DCOx and MODx settings
BCSCTL1 = CALBC1_1MHZ; // Set DCO
DCOCTL = CALDCO_1MHZ;
P1SEL = BIT1 + BIT2 ; // P1.1 = RXD, P1.2=TXD
P1SEL2= BIT1 + BIT2 ; // P1.1 = RXD, P1.2=TXD
UCA0CTL1 |= UCSSEL_2; // SMCLK波特率发生时钟
UCA0BR0 = 104; // 1MHz 9600 波特率发生器分频系数低八位
UCA0BR1 = 0; // 1MHz 9600 波特率发生器分频系数高八位
UCA0MCTL = UCBRS0; // Modulation UCBRSx = 1
UCA0CTL1 &= ~UCSWRST; // **Initialize USCI state machine** 系统复位
IE2 |= UCA0RXIE; // Enable USCI_A0 RX interrupt 开启接受中断
_EINT();
}

#pragma vector=USCIAB0RX_VECTOR
__interrupt void USCI0RX_ISR(void)
{
while (!(IFG2&UCA0TXIFG)); // USCI_A0 TX buffer ready?
UCA0TXBUF = UCA0RXBUF; // TX -> RXed character
}

求解释,拜托了。

  • 你好,

         下面是2553的uart范例程序,建议先试试下面的程序能否进入中断,然后再对比一下你的程序来调试

    #include <msp430.h>

    int main(void)
    {
    WDTCTL = WDTPW + WDTHOLD; // Stop WDT
    if (CALBC1_1MHZ==0xFF) // If calibration constant erased
    {
    while(1); // do not load, trap CPU!!
    }
    DCOCTL = 0; // Select lowest DCOx and MODx settings
    BCSCTL1 = CALBC1_1MHZ; // Set DCO
    DCOCTL = CALDCO_1MHZ;
    P1SEL = BIT1 + BIT2 ; // P1.1 = RXD, P1.2=TXD
    P1SEL2 = BIT1 + BIT2 ; // P1.1 = RXD, P1.2=TXD
    UCA0CTL1 |= UCSSEL_2; // SMCLK
    UCA0BR0 = 104; // 1MHz 9600
    UCA0BR1 = 0; // 1MHz 9600
    UCA0MCTL = UCBRS0; // Modulation UCBRSx = 1
    UCA0CTL1 &= ~UCSWRST; // **Initialize USCI state machine**
    IE2 |= UCA0RXIE; // Enable USCI_A0 RX interrupt

    __bis_SR_register(LPM0_bits + GIE); // Enter LPM0, interrupts enabled
    }

    // Echo back RXed character, confirm TX buffer is ready first
    #pragma vector=USCIAB0RX_VECTOR
    __interrupt void USCI0RX_ISR(void)
    {
    while (!(IFG2&UCA0TXIFG)); // USCI_A0 TX buffer ready?
    UCA0TXBUF = UCA0RXBUF; // TX -> RXed character
    }