This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于MSP430F6733 硬件的问题

各位同事朋友,我有个关于MSP430F673X问题请教大家帮忙!

1、使用TI并口的JATG  仿真器无法找到硬件,如果使用TI的3线SW可以下载,这个为什么?

PIN的2脚接JATG的1脚,3脚接JATG的3脚,4脚接JATG的5脚,5脚接JATG的7脚,6脚接JATG的9脚,7脚接JATG的11脚。

我用F427是可以用并口下载得。

2、如何设置RTCPS0CTL,并且我想知道这个是做什么用得。

3、RTC我看计数模式,和日历模式,是不是二选一。

4、在LPM3模式下是否在走?

5、以下代码CPU 是否工作在16M时钟下?SMCLK是不是4M

UCSCTL6 &= ~XT1OFF; //打开
UCSCTL6 |= SMCLKOFF|XCAP_3;
do
{
UCSCTL7 &= ~(XT2OFFG | XT1LFOFFG | DCOFFG);
SFRIFG1 &= ~OFIFG; // Clear fault flags
__delay_cycles(2000);
} while (SFRIFG1 & OFIFG); // Test oscillator fault flag
__delay_cycles(48000);
__bis_SR_register(SCG0); // Disable the FLL control loop
UCSCTL0= 0; // Set lowest possible DCOx=31, MODx=0
UCSCTL1 = DCORSEL_7; // Select DCO range 24MHz operation
UCSCTL2 |=FLLD_1|(243*2); //16M
__bic_SR_register(SCG0); // Enable the FLL control loop

请各位朋友帮忙解答一下?

 

  • 王树楠,

    1.请问你这里的并口JTAG仿真器用的是什么工具?可否告知详细型号?是指4-wire JTAG吗?你可以参考一下下图看看,链接是否有问题。

    2.RTCPS0CTL寄存器是Real-Time Clock Prescale Timer 0 Control Register,你可以查看一下user guide对应的额RTC_C的寄存器说明部分,尤其是结合“ Figure 24-1. RTC_C Block Diagram”,主要就是用于控制clock预分频,但是在将RTC-C用作real-time clock calendar mode时,RT0PSDIV,RT0PSHOLD值会忽略此寄存器中的值,而会自动设置。故此寄存器主要在32-bit counter mode mode下其作用。

    3. 是的,二者二选一;

    4.不仅在LPM3, 在LPM3.5.下仍就可以工作;

    BR,

    Lina

  • 王树楠,

    5.你的XT1上接的是32768Hz的晶体吧。如果是的话,计算过程为:

    fDCOCLK = D × (N + 1) × (fFLLREFCLK ÷ n)
    fDCOCLKDIV = (N + 1) × (fFLLREFCLK ÷ n)

    看程序应该是N=243, D=2, 默认 fFLLREFCLK=XT1=32768Hz,

    故fDCOCLK = 2*244*32768=16MHz,

    fDCOCLKDIV = MCLK=SMCLK=8MHz

    建议你将MCLK,SMCLK从管脚输出来,用示波器看看是不是这些值。

    BR,

    Lina