TI的工程师好!我这两天在学MSP430G2553的AD模块,其中多通道采样用了DTC功能,对通道11(半电源)和通道10(内置温度传感器)进行采样,一开始定义的数据存储区是一个大小为2的数组,调试总是有问题,后来发现只要采用DTC,指定INCH_X后,就会将INCH_X以下的所有通道都采样并传输到数据存储区中,也就是ADC10AE0失效了?如果是这样的话,那假如我只想采样通道10和11,那么意味着寄存器ADC10DTC1的值至少为12(最高通道为11,总共12个通道,每个通道至少采样一次)?同时数据存储区大小也必须为12?请问是这样理解的吗?谢谢!