This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于MSP430+CC1101+CR2450电池在使用中的问题

Other Parts Discussed in Thread: CC1101

HI

    我有以下问题请教,我的设计为MSP430+CC1101+CR2450纽扣电池,当使用直流电源供电时,系统电压在<2V时可以正常工作,但用CR2450电池时,负载电压在2.4V时已无法正常工作,不知道什么原因。

    如果在直流电源供电的情况下,串联一个100欧姆的电阻,也会发生类似电池供电后的情况,初步判断是电池内阻增大的原因,从设计的角度,请问如何避免这种情况。

谢谢

  • 楼主你好!

    1,楼主指的不能正常工作是什么意思?无法启动?无法收发?还是其他频繁复位?

    2,如楼主所说,有可能是电池内阻变大。建议楼主使用示波器检测下电源电压,是不是在发送接收的时候有电压跌落比较厉害?如果是的话,增加电源的能量储备器件有一定改善作用,例如CBB电容。

  • 你好!

    有两个建议:

    1.拿到CR2450的规格书,上面有放电曲线,设置合理的截止使用电压点;

    2.使用MCU的ADC将电池电压采会去进行检测;

    CR2450的放电截止电压大约在2.5V,正如你分析的那样,在2.4V以下时电池内阻急剧增加,输出电压急剧下降,所以建议系统工作在CR2450的2.6V或者选择一个更高一点的值,保障系统稳定。