This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430F5325之全速跑问题

测试的程序使用官方的程序,将主频升至25M,然后循环外部的IO高低电平变化,断开了仿真器,程序直接运行,发现用不了几分钟就跑死了,IO无变化,将N调低,还是会出现跑死现象

  • 楼主你好!

    系统是怎么供电的?

    试试下面的代码

    void Drv_SetVcoreUp (UINT16_T level)
    {
    PMMCTL0_H = PMMPW_H; /* Open PMM registers for write */
    SVSMHCTL = SVSHE + SVSHRVL0 * level + SVMHE + SVSMHRRL0 * level; /* Set SVS/SVM high side new level */
    SVSMLCTL = SVSLE + SVMLE + SVSMLRRL0 * level; /* Set SVM low side to new level */

    while ((PMMIFG & SVSMLDLYIFG) == 0); /* Wait till SVM is settled */

    PMMIFG &= ~(SVMLVLRIFG + SVMLIFG); /* Clear already set flags */
    PMMCTL0_L = PMMCOREV0 * level; /* Set VCore to new level */

    if ((PMMIFG & SVMLIFG)) /* Wait till new level reached */
    while ((PMMIFG & SVMLVLRIFG) == 0);

    SVSMLCTL = SVSLE + SVSLRVL0 * level + SVMLE + SVSMLRRL0 * level; /* Set SVS/SVM low side to new level */
    PMMCTL0_H = 0x00; /* Lock PMM registers for write access */
    }


    /*
    *********************************************************************************************************
    * Drv_UcsInit()
    *
    * Description : (1) TBD
    *
    * Argument(s) : none.
    *
    * Return(s) : none.
    *
    * Caller(s) : Application.
    *
    * Note(s) : (1) TBD
    *********************************************************************************************************
    */

    void Drv_UcsInit (void)
    {
    // Increase Vcore setting to level3 to support fsystem=25MHz
    // NOTE: Change core voltage one level at a time..
    Drv_SetVcoreUp (0x01);
    Drv_SetVcoreUp (0x02);
    Drv_SetVcoreUp (0x03);

    UCSCTL3 = SELREF_2; // Set DCO FLL reference = REFO
    UCSCTL4 |= SELA_2; // Set ACLK = REFO

    __bis_SR_register(SCG0); // Disable the FLL control loop
    UCSCTL0 = 0x0000; // Set lowest possible DCOx, MODx
    UCSCTL1 = DCORSEL_7; // Select DCO range 50MHz operation
    UCSCTL2 = FLLD_1 + 762; // Set DCO Multiplier for 25MHz
    // (N + 1) * FLLRef = Fdco
    // (762 + 1) * 32768 = 25MHz
    // Set FLL Div = fDCOCLK/2
    __bic_SR_register(SCG0); // Enable the FLL control loop

    // Worst-case settling time for the DCO when the DCO range bits have been
    // changed is n x 32 x 32 x f_MCLK / f_FLL_reference. See UCS chapter in 5xx
    // UG for optimization.
    // 32 x 32 x 25 MHz / 32,768 Hz ~ 780k MCLK cycles for DCO to settle
    __delay_cycles(782000);

    // Loop until XT1,XT2 & DCO stabilizes - In this case only DCO has to stabilize
    do
    {
    UCSCTL7 &= ~(XT2OFFG + XT1LFOFFG + DCOFFG);
    // Clear XT2,XT1,DCO fault flags
    SFRIFG1 &= ~OFIFG; // Clear fault flags
    }while (SFRIFG1&OFIFG); // Test oscillator fault flag
    }

  • 我是3.3V供电,代码和上面一致

  • ACLK,SMCLK为外部晶振32.768k和4M

  • Stanford Chen ,

    请问在3.3V供电的基础上,在主频设置为25MHz之前,有否将MSP430F5xxx系列的 core-level升高?默认core-level为0,一般而言,最高能支持主频8MHz。若想运行至25MHz的话,得将core-level升高至3。建议使用core library。

  • 已升高core-level升高至3,跑了一个晚上,发现跑飞了

  • 频率降至20M,正在测试中,半小时内没出现跑飞现象

  • 建议楼主把自己的代码和MCU周边原理图贴出来。