This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi all,
我在使用5418A定时器实现定时任务。遇到以下问题,请教专家:
1. 我可以用TAxCCR0 TB0CCR0实现定时,比如点亮LED,但是实际当中CCR0需要实现捕获功能。请问在实现捕获功能的同时,可以实现定时功能吗?
2. 我试过几次用其他的CCRx实现定时功能,但是不管用。请问应该如何配置?
Thx
Nick
Nick,
您好,
1、可以用CCR0做捕获,用CCR1做计时;
2、可以参考MSP430F5418A的code example中的ta3_08.c
Nick,
您好,
1、可以用CCR0做捕获,用CCR1做计时;
2、可以参考MSP430F5418A的code example中的ta3_08.c