This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Reading Code File ........................... done
-- Code size = 0x012E ( 302 ) bytes
=====================================
JTAG communication initialization.... OK
Verifying Security Fuse .................... OK
Reading Retain Data ............. done
Erasing memory ............................... done
Verifying Retain Data ...................... done
JTAG communication initialization.... OK
Flash programming .................... done
Verifying check sum ......................... OK
DCO constants verification....... failed
--------------- FAILED !!! -----------------
在烧录程序的时候出现了这个错误
提示FAILED
用的是430G2211的芯片
用430G2452的烧录就没问题,430G2452和430G2211的晶振配置是不是不一样啊,用到底层的也就是时钟的配置
DCO constants verification....... failed
程序比较简单,也就是这里用到的是底层,其他的都是标准的C语言了
具体该怎样解决啊
这里有两个问题:
第一:所有TI出厂的芯片都会对每个芯片进行DCO校准。每个芯片的校准值理论上不具有任何一致性。从别的芯片读出来的校准值是别的芯片的。即使烧到别的芯片里,能跑起来,也失去了DCO校准的意义。如果你只是在调试时遇到这种问题,那麻烦你换颗芯片。但是如果是量产时出现误擦除,为了保证DCO的频率精度,必须重新校准。
第二:你是从G2452导入的程序运行正常,然后想要换个G2211芯片来运行吗?G2452出厂时TI提供完成的几组DCO频率的校准值,如下
而低成本的G2211我们在出厂前只提供一组1M频率下的校准值,如下
因此如果你在G2452的代码上有尝试去读取非1M频率的值时是正常的,但是在G2211上这个值就是FF。
你可以自己检查下